Chicago,
12
October
2023
|
17:09
Europe/Amsterdam

Littelfuse complete solutions now available through Newark

FAR 974 Inline

Newark partners with Littelfuse to offer customers a one-stop-shop for all their project requirements. Littelfuse is a diversified industrial technology manufacturing company committed to creating a sustainable, interconnected, and safer world. The products available from Newark include fuses, circuit breakers, surge protectors, TVS diodes, Thyristors, Diodes, MOSFETs, IGBTs, Gate Drivers, power modules, switches, and sensors.

Littelfuse circuit protection products play a crucial role in safeguarding electrical systems and personnel. Their offerings provide protection against electrostatic discharge, power surges, short circuits, voltage spikes, arc flash, and other harmful occurrences. In addition, Littelfuse offers a comprehensive portfolio of advanced power semiconductor technologies, including silicon and wide band gap solutions in discrete and module packages. Littelfuse also provides a broad platform of technologies that sense proximity, flow, speed, temperature, and fluid level, which are ideal for complex electronic systems.

Jose Lok, Product Category Director, Semiconductors, said: “We are delighted to partner with Littelfuse. This collaboration will enable our customers to access their comprehensive range of solutions, simplifying the procurement process and accelerating their time to market."

Littelfuse's extensive product portfolio supports several sectors such as automotive, consumer, industrial, building solutions, medical devices, aerospace, and data centre & cloud. Some of the best-selling products available at Newark include:

  • High side/ low side gate driver LF2181N: The LF2181N is a high voltage, high speed gate driver capable of driving N-channel MOSFETs and IGBTs in a half bridge configuration. The process technology enables the LF2181N’s high side to switch to 600V in a bootstrap operation. The LF2181N logic inputs are compatible with standard TTL and CMOS levels (down to 3.3V) to interface easily with controlling devices. The driver outputs feature high pulse current buffers designed for minimum driver cross conduction. The LF2181N is offered in SOIC(N)-8 package and operate over the extended temperature range of -40 °C to +125 °C.
  • USP10973 Thermistor Assembly: This copper probe assembly is suitable for a wide range of temperature sensing applications. It has a tight tolerance, is moisture resistant, and has PVC insulated lead wires. The maximum operating temperature is 105°C.
  • DST Series: DST series Ultra Low VF Schottky Barrier Rectifier is designed to meet the general requirements of commercial and industry applications by providing high temperature, low leakage and lower VF products. It is suitable for high frequency switching mode power supply, free-wheeling diodes and polarity protection diodes.

Littelfuse solutions are available to purchase from Farnell in EMEA, Newark in NA and element14 in APAC.

Boilerplate

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production. Farnell Global helps its customers access the products and services they need 24/7. With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell Global provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific. It also sells through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com