Chicago,
26
October
2023
|
16:38
Europe/Amsterdam

Newark empowers engineers with Superior Sensor Technology's cutting-edge pressure sensors

Superior Sensor Technology's NimbleSense architecture offers engineers a fully integrated solution for pressure sensing, delivering higher accuracy and application-specific capabilities right out of the box.

FAR 999 Inline

Newark has announced a distribution agreement with Superior Sensor Technology, a pioneer in application-specific pressure sensors for the medical, industrial, and HVAC markets.

Engineers are often faced with the challenge of finding customizable pressure sensor systems for their specific applications. Traditional sensors require significant time and effort for customization, which can sometimes lead to project delays.

Superior Sensor’s products are based on their proprietary NimbleSense architecture that turns the pressure sensor into a fully integrated module that combines a MEMS sensor with additional circuitry and software. Superior Sensor's NimbleSense architecture delivers fully integrated solutions with application-specific capabilities, making it a more efficient and cost-effective option for engineers.

Anthony Gioeli, Vice President of Marketing at Superior Sensor Technology said: “We are proud to offer engineers pressure sensors with a modular architecture providing unique features based on the end application. Our core technology has an impressively low noise floor, ensuring higher accuracy. With our ability to integrate advanced functionality like closed loop control, pressure switch, notch filter, and advanced digital filtering, our sensors eliminate the need for external designs.

“Customers can also take advantage of programmable features like bandwidth filtering and variable pressure ranges allowing our customers to further optimize their pressure sensors."

Superior Sensor Technology provides a range of application-specific pressure sensors for various industries, including HVAC, industrial use cases, medical ventilators, CPAP machines for sleep apnea, spirometers, and UAVs.

Superior Sensors products are now in stock at Farnell in EMEA, Newark in North America and element14 in APAC.

Boilerplate

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production. Farnell Global helps its customers access the products and services they need 24/7. With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell Global provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific. It also sells through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com