Newark emphasizes precision with Analog Devices signal chains
Industrial automation, energy monitoring and test and measurement sectors all to benefit from extreme accuracy
Newark has announced that it has added the full range of precision signal chains from Analog Devices, Inc. (ADI), to help users create the optimum end-solution for multiple applications. From sensors to bits, customers can find and tailor solutions that are optimized for demanding applications. The signal chains are available to order directly from the Newark website.
Jose Lok, Product Category Director, Semiconductors from Newark, said, “Newark is positioned to enable developers to integrate ADI technology into their designs, which greatly accelerates time to market. Development engineers can use ADI’s high-precision signal chains to optimize their solutions for demanding electrification, automotive, digital health, instrumentation, smart industry, energy and sustainability applications.”
Precision signal chains now available from Newark include:
- Precision Current Sensing: These signal chains can be used to tackle challenging current measurement tasks in applications.
- Precision High Voltage: ADI’s precision high voltage signal chains combine precision high voltage amplifiers, high voltage digital-to-analogue converters (DACs), difference amplifiers and matched resistor networks.
- Isolated Gate Drive and Sense: These sense signal chains combine robust switch control and scalable multichannel monitoring into a flexible solution covering a range of AC/DC and DC/AC applications.
- Precision Low Power: ADI’s precision low power signal chains are designed and optimized for small-size battery-powered or power sensitive applications.
- Precision Narrow Bandwidth: ADI offers precision narrow bandwidth signal chains that focus on optimizing the performance of systems where the signals of interest are in the range of DC to approximately 10 kHz.
- Precision Medium Bandwidth: Precision medium bandwidth signal chains cover a large range of applications that demand accuracy across signal bandwidths from DC to 500 kHz, with sampling rates up to 4 MSPS.
- Precision Wide Bandwidth: The precision wide bandwidth signal chains bring the insight and flexibility needed to optimize application specific parameters for measurement and drive solutions.
Sabine Colen, Director, Global ecommerce Channel from Analog Devices adds, “The benefits from ADI's precision technology signal chains stem from the fact that these signal chains come complete with customizable solutions, purpose-developed knowledge bases that have been developed from more than 50 years of experience and expertise.”
Precision technology signal chains are now available from Newark in North America, Farnell in EMEA and element14 in APAC.
Boilerplate
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production. Farnell Global helps its customers access the products and services they need 24/7. With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell Global provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific. It also sells through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com