Chicago,
12
March
2024
|
05:30
Europe/Amsterdam

Newark now stocking Traco Power's compact 5-50 Watt encapsulated TMPW Series

Electronics and industrial design engineers can benefit from these ultra-compact AC/DC power supplies, available in PCB and chassis mount packages, for demanding building automation, industrial, and IT applications.

FAR 1035 Inline

Newark is now stocking the TMPW Series of ultra-compact AC/DC power supplies from Traco Power.

The 5-50 Watt encapsulated power supplies are available in both PCB and chassis mount packages. The chassis mount models come with screw terminals or optional JST connectors and have an extended input range of 90 – 305 VAC, making them ideal for use in a wide range of industrial and household/building applications.

Other features of the TMPW series include an I/O-isolation voltage of 4000 VAC, operating temperature range of –40°C to +70°C, and Class II safety approvals. Additionally, an internal EN 55032 Class B filter saves valuable space for an otherwise often mandatory external filter. The series is also ERP ready, which means that it has an energy-efficient design, with less than 0.1 Watt standby power consumption, and satisfies tomorrow's requirements for compact green power applications around the globe.

Newark Product Segment Leader for Traco Power, Steve Hallgate, said, “The TMPW Series of AC/DC power supplies from Traco Power is an excellent addition to Newark's power portfolio. With their compact size, extended input range, and energy-efficient design, these power supplies are sure to be a hit with engineers and designers alike.”

Traco Power’s TMPW series can be ordered online from Newark in North America, Farnell in EMEA, and element14 in APAC.

Boilerplate

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production. Farnell Global helps its customers access the products and services they need 24/7. With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell Global provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific. It also sells through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com