Phoenix,
19
February
2026
|
14:00
Europe/Amsterdam

Newark expands automated test portfolio with new cost-effective NI PXI systems from Emerson

FAR 1194 Inline

Newark has announced the availability of a new range of NI PXI hardware from Emerson, designed to lower the cost barrier for high-performance automated testing.

This expansion provides engineers with an affordable entry point to the industry-standard PXI platform while maintaining the precision, synchronization and robust software integration that are hallmarks of NI technology

"Our partnership with Newark continues to be a cornerstone of Emerson’s mission to deliver scalable, high-performance test solutions to engineering teams worldwide," said Brandon Treece, Director of NI PXI Product Marketing at Emerson. "With the launch of our new, affordable NI PXI hardware, we’re making it easier than ever to build adaptable, cost-effective automated test systems—delivering software-driven flexibility, measurement precision, and system scalability to drive innovation forward."

The new hardware suite, optimized for use with LabVIEW, InstrumentStudio, and TestStand, includes:

  • NI PXIe-5108 Oscilloscopes: 4- and 8-channel options with 100 MHz bandwidth and 14-bit resolution for high-density measurements.

  • NI PXIe-1081 Hybrid Chassis: cost-effective 18-slot chassis optimized for high-channel-count, low-throughput applications.

  • NI PXIe-8842 / 8862 Controllers: simplified embedded controllers supporting Windows 11 and NI Linux Real-Time for flexible system integration.

  • NI PXIe-6381 / 6383 DAQ Modules: first 18-bit PXI Express multifunction I/O devices, offering precise, low-noise voltage measurements.

Anthony Coletto, Vice President, Supplier Management at Newark said: “These new NI PXI modules remove the trade-off between power and price. By lowering the cost of entry, we are helping more engineers deploy the industry’s most trusted synchronization and software tools for their automated test systems.”

The new NI PXI hardware range is available to order from Newark in North America, Farnell in EMEA, and element14 in APAC.

Boilerplate

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production. Farnell Global helps its customers access the products and services they need 24/7. With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell Global provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific. It also sells through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com