Newark now stocking TE Connectivity’s latest automation solutions
The keys to accelerated automation projects and industrial productivity are now in stock
Newark has expanded its industrial automation solutions portfolio with the latest offerings from TE Connectivity (TE), a global leader in connectivity and sensor solutions. Engineers can now access a broad range of cutting-edge products designed to elevate the intelligence, reliability, and efficiency of modern automation systems.
As industrial environments demand faster, smarter, and more connected solutions, TE’s advanced products provide the backbone of high-performance factory automation.
The selection largely comprises the central nervous system of industrial automation systems. From high-speed connectors helping enable 25 Gbit/s data transfer to finely engineered relays that think before they switch as well as advanced sensors and intelligent power solutions, TE Connectivity’s advanced solutions enable machines to communicate, adapt, and deliver.
From designing advanced robotics to integrating high-voltage power systems or industrial IoT scaling, Newark’s extensive range of TE Connectivity products helps ensure its customers have access to resilient connections, smart controls, and exceptional reliability.
Standout products from the new range include:
ERNI SMC Connector: This highly reliable and high contact density connector for BtB (Board to Board) and WtB (Wire to Board) with small multiple connectors is available in a wide range of shapes to enable different mating configurations.
Force Guided and RT/RZ Series Relays: The relays are designed for safety circuits in combination with, for example, light curtains, interlock switches, emergency stop switches, and control outputs.
AMPMODU 2mm connectors: The AMPMODU 2 mm interconnection system reliably and economically meets the requirements of today’s miniature, sophisticated electronics. This system is highly suitable for space constrained environments with design features that enable reliable signal transfers in demanding applications.
High Voltage Battery Disconnect Switches: KISSLING High Voltage (HV) battery disconnect switches are robust safety solutions that are now available in multiple versions: 250A (without high voltage Interlock) and 400A / 500A (with high voltage interlock).
To learn more about the full range of TE Connectivity solutions available at Newark, visit https://www.newark.com/te-connectivity-automation-control.
Boilerplate
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production. Farnell Global helps its customers access the products and services they need 24/7. With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell Global provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific. It also sells through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com