Phoenix,
05
November
2026
|
14:00
Europe/Amsterdam

Newark launches Panasonic ERJPC Series: Thin-film precision in a thick-film footprint

FAR 1224 Inline

Double Power Density enables smaller designs with accuracy down to 0.1% and 25ppm stability

Newark is now selling the new ERJPC series of super high-precision thick-film resistors from Panasonic Industry. This innovative product line delivers precision levels previously only achievable with thin-film technology, offering engineers a powerful new tool for space constrained and high accuracy designs.

The ERJPC series delivers a TCR as low as 25ppm/K and tolerances down to ±0.1% and ±0.5%, allowing designers to achieve thin-film precision within a more cost-effective thick-film architecture. With up to double the power density of traditional thin-film solutions—0.2W in a 0603 size and 0.25W in 0805—designers can shrink their layouts by replacing larger components with smaller ERJPC resistors.

Key Specifications Precision

  • Tolerances of ±0.1% and ±0.5%

  • Stability: TCR down to 25ppm/K

  • Power Density: 0.2W (0603) and 0.25W (0805)

  • Reliability: AEC-Q200 compliant and RoHS certified

  • Applications: Battery Management Systems, Engine Control Units, Industrial Automation, and Consumer Electronics

Clara Lagomarsini, Product Manager Device Solution Business Division at Panasonic Industry explains: “Many applications - such as Battery Management Systems (BMS), Electronic Control Units (ECUs), home appliances and industrial and factory automation systems - require high precision components. Our thick film technology is a real alternative to thin film implementations. The new ERJPC thick-film series combine high-precision, environmental stability, while offering a new path towards long-term cost efficiency.”

Andy Weatherill, VP Global Product, Supply Chain, Newark, said: “Adding ERJPC to our Panasonic portfolio gives customers a high‑precision solution. By using advanced materials and optimized structures, Panasonic enables engineers to achieve thin‑film‑level accuracy alongside the power‑density advantages of thick‑film technology — supporting meaningful board downsizing and long‑term cost savings in demanding designs.”

The Panasonic ERJPC Super High-Precision Thick-Film Resistor series is available for fast delivery from Newark in North America, Farnell in EMEA, and element14 in APAC.

Boilerplate

Boilerplate

Farnell Global is a fast and reliable distributor of electronic components. By connecting design, sourcing, and supply, Farnell Global helps Engineers and Buyers make the right decisions quickly and with confidence.

As a high-service electronics distributor, Farnell Global supports customers across the full lifecycle through product availability, local expertise, close collaboration with leading suppliers, digital and eProcurement tools, and fast and reliable delivery.

With more than 80 years of experience, 48 localised websites, dedicated team of over 3,000 employees and over one million products in stock from more than 2,000 authorised manufacturer brands, Farnell Global provides every component its customers need to build the technology of tomorrow. 

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific.  It also sells through its CPC business in the UK. 

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design. 

 For more information, visit http://www.farnell.com