Chicago,
18
April
2023
|
13:54
Europe/Amsterdam

Analog Devices’ Multichannel System Clocking Device now available from Newark

FAR913_ ADI inline

The AD-SYNCHRONA14-EBZ is an ideal self-contained device to use in evaluation and prototyping of applications that need a highly accurate frequency and phase-controlled source clock. It is designed around the Analog Devices AD9545 and HMC7044 and greatly simplifies clock distribution and multi-channel synchronization in complex systems. 

The AD-SYNCHRONA14-EBZ is intended to be used by trained professionals in a laboratory environment, and not intended as an end product for commercial use. It can be taken as a complete reference design and customised as required for any end customer applications. Full design details are made available free of charge. 

The device comes in a 1U mechanical form factor and uses industry-standard SMA and TwinAX connectors that are commonly found in labs. Its applications include: 
• High accuracy reference clock distribution 
• Systems clocked from a single source 
• Clocks derived from 100MHz or 122.88MHz 
• Phased Array Systems, RADAR, EW, SATCOMS, SDR 
• Bench Equipment 
• Remote controlled operation 

Analog Devices’ evaluation board can be purchased from Farnell in EMEA, Newark in North America and element14 in APAC. 



 

Boilerplate

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production. Farnell Global helps its customers access the products and services they need 24/7. With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell Global provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific. It also sells through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com