Newark and Transphorm announce a global SuperGaN device distribution agreement
Newark customers now able to fully benefit from rapid access to future-proofed SuperGaN power FET portfolio
Newark has announced a new global distribution partnership with Transphorm, a world leader in the design and manufacturing of highly robust high-voltage GaN (gallium nitride) semiconductors for power conversion applications.
Transphorm’s high performance, high-reliability SuperGaN® power semiconductors leverage one of the largest power GaN IP portfolios (1,000+ patents) within the widest variety of device packages. This technological expertise is harnessed in a normally-off d-mode GaN platform that delivers best-in-class robustness and reliability. End products using SuperGaN FETs gain several advantages such as higher power density and efficiency along with lower total power system cost versus alternative solutions.
The above and other application advantages are made possible by the SuperGaN platform’s fundamental physics. These physics drive game-changing innovations available today and slated for the future—resulting in Transphorm’s GaN being a versatile, future-proofed GaN solution.
Newark Product Category Director, Passives & Semiconductors, Jose Lok, said, “Onboarding Transphorm as a new supplier supports our commitment to deliver high quality products to customers while giving them the ability to choose preferred manufacturers as well as the best GaN device package and performance to meet their design needs.”
Benefits of Transphorm's SuperGaN Devices include:
- Industry-leading efficiency (over 99%)
- Up to 50% higher power density
- Up to 20% lower system cost
- Proven robustness and reliability
- Drop-in and/or drive compatible with all other high voltage power technologies
- Supports a wide range of power applications (from 40W to 7.5kW, with higher power ratings coming soon)
Transphorm’s GaN innovations have led to several industry firsts, such as the 1200 V GaN-on-Sapphire device slated for commercial availability mid-2024; short-circuit withstand times of five microseconds; and a GaN four quadrant switch with true voltage and current bidirectionality control.
Lok added, “The primary advantage of SuperGaN is the use of GaN in its native d-mode form. By doing this, the 2DEG channel that is spontaneously created between the undoped GaN and AlGaN layers is left untouched. This yields a simple-to-manufacture solution that harnesses all the 2DEG’s inherent advantages, maximizing the device’s electron mobility and charge while minimizing temperature effects. The result is the highest performing solution spanning the widest power spectrum versus other Si and WBG technologies. These are just some of the many reasons we are now delighted to offer them, with rapid ordering and delivery options, to our customers.”
“The power electronics market across all industries is radically changing as power conversion technologies like our SuperGaN platform drive major design and performance advantages,” said Vipin Bothra, VP of sales for North America and Europe at Transphorm. “Our GaN devices are currently being adopted into a global consumer, industrial and automotive markets. We feel it is critical to enable our customers to access our devices however they prefer. Partnering with well-respected global distributors like Newark is a necessary step to meeting that objective. We look forward to a strong, mutually beneficial relationship that helps revolutionize power systems in everything from adapters and PCs to renewable energy systems and electric vehicles.”
For more information about Newark and its extensive range of SuperGaN products, visit https://www.newark.com/b/transphorm.
Boilerplate
Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production. Farnell Global helps its customers access the products and services they need 24/7. With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell Global provides every component its customers need to build the technology of tomorrow.
Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific. It also sells through its CPC business in the UK.
Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.
For more information, visit http://www.farnell.com