Chicago,
29
August
2019
|
16:00
Europe/Amsterdam

Newark Now Stocking Kitronik Products and Accessories for micro:bit, Arduino and Raspberry Pi

Kitronik enables project creation and inspires imagination in STEM education

FAR477_Kitronik_inline

Newark, the Development Distributor, is now stocking Kitronik products; an exciting range of accessories for micro:bit, Arduino and Raspberry Pi, perfect for educators, students, makers and hobbyists.

Kitronik products encourage imagination and creativity when used in conjunction with the latest generation of open-source programmable computer boards. The kits and accessories enable interaction between programming and hardware, making them ideal for developing computational thinking skills in younger students. This new partnership with Kitronik enhances Newark’s range of products for education and builds upon its position as the exclusive manufacturer and distributor of the BBC micro:bit, the largest manufacturer and distributor of Raspberry Pi boards and major stockist of Arduino boards.

Kitronik products can be used to support STEM education in classrooms and after school clubs and seek to engage and inspire students of all abilities to further their knowledge of electronics, coding and design. Newark stocks everything required to get started in physical computing for both education establishments and independent coding clubs.

Kitronik products and accessories for the micro:bit in stock at Newark include:

  • The Inventors Kit  provides an introduction to programming and hardware interaction and contains everything required to carry out ten experiments with the micro:bit, using LEDs, motors, light sensors and capacitors. The kit includes an easy to follow tutorial book and no programming experience or soldering is required. Circuits can be completed in minutes.
  • The MOVE mini buggy kit provides a fun introduction to robotics making a two-wheeled robot that is suitable for autonomous operation. It is perfect for remote control projects via Bluetooth applications or control using a second micro:bit. Five RGB individually addressable Zip™ LEDs are included which can be used as indicators, and a pen can be attached to the robot to draw shapes. Kitronik’s custom code blocks for the Servo:Lite motors are available to make the task of coding as quick and painless as possible.
  • The Kitronik: GAME ZIP 64 is the ultimate retro gaming accessory for the BBC micro:bit. It has been designed to be an all in one hand-held gaming platform, which includes a built-in, 64 (8x8) individually addressable full colour Zip™ LED screen. It features on-board sound, four directional buttons, two fire buttons, haptic feedback, and breakout points so that shoulder buttons or I2C devices can be added. All of these features are fully programmable and breakout points are available to allow for the use of larger LED screens.

Courtney Kennedy, Technology Solutions Marketing Manager at Newark says “The addition of Kitronik further broadens our existing wide range of open-source educational and STEM products. The Kitronik range provides educators with new and creative ways to inspire students to get involved in physical computing, providing easy access to devices that enable them to promote the development of key skills such as computational thinking.”

Newark’s support for the development of the next generation of electronics engineers includes free resources, including lesson plans, project ideas and more, available on the Newark website. Newark has a broad range of products within its product range that promote learning about physical computing, an important way for children to develop computational thinking and team working skills.

The Kitronik products and accessories for micro:bit, Arduino and Raspberry Pi are available from Newark.

Boilerplate

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production. Farnell Global helps its customers access the products and services they need 24/7. With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell Global provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific. It also sells through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com

Download