Chicago,
04
April
2023
|
15:55
Europe/Amsterdam

New NI PXI Bundles now available from stock at Newark

Bundles are the ideal, cost-effective way to get started with PXI to automate high-quality measurements and testing

far906_featured NI PXI

Newark is now supplying new PXI test and measurement bundles from NI.

Each high-performance bundle includes a PXI Instrument in a 5-slot PXI system that is controlled through a Thunderbolt™ USB-C port, making them an ideal, cost-effective way to automate high-quality measurements and testing with PXI. Direct connection to a laptop eliminates the additional cost of an on-board controller, providing an economic first-time investment into PXI. Each bundle includes one instrument, leaving four remaining slots to add instruments as testing needs evolve.

For more than 40 years, NI has developed automated test and measurement systems that help engineers solve the world’s toughest challenges. The company’s PCI eXtensions for Instrumentation (PXI) are the industry-standard and can be used to build high-performance, mixed measurement systems for validation and production tests. Combining multiple box instruments into a sub-compact single system, without compromise on performance, PXI software connectivity offers scalability and flexibility that enables users to customise measurements and simplify test development.

NI's software environment for PXI, which includes LabVIEW and TestStand, allows engineers to easily customize testing procedures and data acquisition, analysis, and reporting to meet their specific needs. PXI’s high performance, value, modularity and software connectivity has seen it deployed across many industries including automotive, aerospace, electronics, semiconductors, life sciences and more.

The architecture of the PXI platform enables users to easily add or remove modules to meet their specific testing requirements. The PXI bundles are based on common applications and configured so that the user can also customize for their particular application by adding modules that fit their requirements. PXI portfolio includes oscilloscopes, source measurement units, LCR meters, waveform generators, digital multimeters and more—that can replace traditional box instruments and with which you can integrate PXI switches in a variety of topologies.

Key benefits include:

  • Open industry standard: With more than 60 vendors offering PXI hardware, engineers have a wide range of options when it comes to selecting modules for their test and measurement needs.
  • High performance: NI PXI hardware utilizes the latest technology, incorporating powerful multicore processors, FPGAs, and other technology to increase measurement range and performance.
  • Scalable: PXI’s architecture makes it possible to synchronize measurements across multiple modules or multiple chassis, enabling systems to grow as requirements change.

“NI’s PXI offers unmatched modularity, flexibility and performance for creating custom test and measurement systems, allowing users to easily tailor their testing systems to their specific needs. These bundles are based on very common T&M applications yet allow the customer to add options to focus on the testing that is important to them,” said James McGregor, Global Head of Test, Tools and Production Supplies at Newark. “With a powerful software environment, users can rapidly develop, customise and confidently deploy testing procedures. This addition to Newark’s portfolio expands and improves an already leading test and measurement range.”

The new NI PXI test and measurement bundles are now available from stock at Farnell in EMEA, Newark in North America and element14 in APAC.

Boilerplate

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production. Farnell Global helps its customers access the products and services they need 24/7. With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell Global provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific. It also sells through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com