Chicago,
15
May
2019
|
00:55
Europe/Amsterdam

Premier Farnell Expands Range of Test and Measurement Products with GW Instek Test Instruments

Inline

Premier Farnell, the Development Distributor, has further expanded the breadth and depth of its product portfolio by adding the GW Instek test & measurement instruments to its range. The products which include programmable power supplies, electrical safety testers, signal sources and power analysers offer customers excellent quality at affordable cost.

Key GW Instek products to be stocked by Premier Farnell include:

  • The APS-7050 programmable linear AC power source - Offering output ratings of 500 VA, 310 V RMS, 2.1 A and a frequency range from 45 to 500 Hz with LAN and USB interfaces. The APS-7050 is ideally suited to producing complex waveform and transient waveform to verify electronic product operation under adverse conditions. Typical applications include production testing in the LED industry and in standby mode power consumption.
  • The GPT-9603 electrical safety tester- Used for testing AC/DC withstand voltage and insulation resistance; the GPT-9600 series AC 100VA AC/DC withstand voltage/insulation resistance tester offers an affordable solution for supporting routine tests of major items to safety standards such as IEC, EN, UL, CSA, GB, JIS and other safety regulations. It is equipped with a PWM amplifier to impede influence from input AC voltage fluctuation and ensure a stable voltage output, providing users with an intuitive operation environment by a simple and clear panel layout, large LCD display and colour LED indicators.
  • The MFG-2110 10 MHz function generator - Part of the MFG2000 series, which includes the MFG-21XX entry-level models and MFG-22XX advanced models. The output channels of MFG-21XX models include one single-channel 10 MHz arbitrary generator and one 25 MHz pulse generator. All instruments feature a 4.3-inch TFT colour display.

“The addition of the GW Instek range of products provides greater choice for our customers through a wider offering of test and measurements products”, says James McGregor, Global Head of Test & Tools at Premier Farnell. “GW Instek has an industry reputation for quality, reliability, affordable prices and ease of use. These products are incredibly competitively priced and help electronics manufacturers to reduce testing costs and increase their productivity.”

The GW Instek products are now available from Farnell in EMEA, Newark in North America and element14 in APAC.

Boilerplate

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production. Farnell Global helps its customers access the products and services they need 24/7. With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell Global provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific. It also sells through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com

Download