Chicago,
09
July
2024
|
06:45
Europe/Amsterdam

Newark Now Stocks Murata's UWB and LoRa Modules for Simplified Wireless Integration

FAR 1077 Inline

Newark is now offering Murata's latest UWB and LoRa connectivity modules for convenient wireless integration. These cutting-edge modules are designed to simplify wireless development and certification, making it easier to incorporate wireless capabilities into a wide range of applications.

Murata's UWB modules provide high-accuracy location functionality with UWB tag and anchor functions in compact packages. These modules feature integrated RF front ends, simplifying the implementation process and reducing the need for extensive RF expertise. This allows developers to seamlessly incorporate advanced location capabilities into their applications.

Additionally, Murata's LoRa modules offer a compact, integrated solution with an embedded MCU. Developers have the flexibility to utilize the MCU as the Host for an End Node, providing customization possibilities for various projects.

"We are pleased to announce the availability of Murata's connectivity modules at Newark," said Ross Murgatroyd, Global Product Segment Leader for Microcontrollers & Wireless at Newark. "These modules represent a significant advancement in wireless connectivity technology and will empower developers to create innovative and robust wireless solutions across diverse industries."

Murata's UWB modules provide unparalleled location accuracy and open up a world of possibilities for asset tracking and RTLS applications. The technology enables location accuracy in the order of 0.1m for indoor or outdoor applications. The UWB Modules available at Newark include:

  • FiRa certified UWB module, Type 2BP is the ultra small UWB module which includes NXP's SR150 UWB chipset, clock, filters and peripheral components. Ideally suited for general IoT devices including battery operated devices.
  • UWB module with integrated BLE wireless MCU, Type 2AB is designed as ultra-small, high quality and lower power consumption module. It can be operated on the wireless MCU making this a suitable part for wearables and applications where size is critical
  • UWB tag module with integrated BLE wireless MCU. Type 2DK is an all-in-one UWB + Bluetooth® LE combo module which integrates NXP Trimension™ SR040 UWB Chipset, NXP QN9090 Bluetooth® LE + MCU chipset, on board antenna and peripheral components. Ideally suited for UWB Tag/Tracker which operates by coin-cell battery, and general IoT devices.

The Murata Type 1SJ LoRa Modules are some of the smallest LoRa Modules in the line-up and include the Semtech SX1262 LoRa ConnectTM Transceiver IC and ST Microelectronics STM32L0 MCU to provide customers with a Regulatory Certified Module that can be used as the core of a LoRa End Node product design. The LoRa modules available at Newark include:

Customers can purchase Murata modules from Newark in North America, Farnell in EMEA and element14 in APAC.

Boilerplate

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production. Farnell Global helps its customers access the products and services they need 24/7. With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell Global provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific. It also sells through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com