Phoenix,
08
October
2024
|
14:43
Europe/Amsterdam

Newark introduces the Raspberry Pi AI Camera

The latest innovation from Raspberry Pi supports on-board camera processing for a variety of popular neural network models

FAR 1101 Inline

Newark has introduced the new Raspberry Pi AI Camera, the latest innovation from Raspberry Pi that expands Newark’s range of artificial intelligence devices.

At a cost of approximately $70 USD, the Raspberry Pi AI Camera - a collaboration with Sony based on its IMX500 Intelligent Vision Sensor - features on-module processing that is compatible with the entire Raspberry Pi single-board computer (SBC) range. The Raspberry Pi AI Camera simplifies complex AI tasks at the edge because all processing is done on the Raspberry Pi AI Camera module itself, leaving the processor in the host Raspberry Pi SBC free to perform other operations.

Simon Wade, Senior Global Product Manager, Single Board Computing at Newark, said, ”This new AI camera module is a remarkable addition to the Raspberry Pi range. As AI-driven applications proliferate across many industries, it shouldn’t surprise anyone that Raspberry Pi and Sony are leading the way to bring optic processing power to the edge. No matter which Raspberry Pi SBC you use, it is compatible with the AI Camera module.”

The camera itself features Sony’s 12MP IMX500 Intelligent Vision Sensor with an integrated low-power inference engine that is pre-loaded with the MobileNet machine vision model. Its 76-degree field of view includes a manually adjustable focus; and comes equipped with 200mm cables for easy connection with any Raspberry Pi SBC.

Wade added, “Raspberry Pi 5 is already highly regarded for its extraordinary processing intelligence, and the ability to effortlessly add the Raspberry Pi AI Camera is further evidence of the board’s exceptional versatility. The benefit to individual developers, casual hobbyists, or large industrial complexes is that it delivers powerful compute power to where it’s needed most, at the edge.”

The Raspberry Pi AI Camera is now available and shipping from Newark in North America.

Boilerplate

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production. Farnell Global helps its customers access the products and services they need 24/7. With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell Global provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific. It also sells through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com