Chicago,
27
June
2019
|
16:00
Europe/Amsterdam

Newark Adds Micro-B Connectors from Amphenol Industrial Operations

Amphenol Micro B connectors_large

Newark, the Development Distributor, continues to offer its community of designers with the varied connector options they need to advance their designs with the addition of the Micro-Bayonet (Micro-B) connectors from Amphenol Industrial Operations. This product line provides an affordable alternative to connectors used in industrial markets requiring high signal counts and small packages.

The Micro-B series offers lightweight, high performance connectors with a small footprint that utilize a robust triple bayonet coupling, providing quick and positive locking. The Micro-B series is ideal for industrial designers seeking high electrical performance at a low price. The new circular connector series is designed for industrial applications such as Telecommunications, HEV, Robotics/Factory Automation, Industrial Instrumentation, Security, and Test Equipment where electrical performance must be met with affordability.

Micro-B meets the requirements of today’s electrical equipment by delivering excellent shell-to-shell electrical bonding for EMI required in rugged connectors. The compact Micro-B features high density insert patterns with size 22D contacts allowing for more circuits to be connected and a simplified termination process with tape and reel contacts. It also offers tool-less and fast mating for ease of use in the field.

Further technical information:

  • RoHS-compliant circular connector series
  • Various mounting options available, including in-line and 2-hole flange mount configurations
  • Operating temperature of -40°C to +125°C, a dielectric withstanding voltage of 500 VRMS and a current rating of up to 3 Amps per contact. It is durable up to 500 mating cycles
  • With Gray ZnNi plating, Micro-B can withstand up to 500 hours salt spray without corrosion detrimental to its operation

Amphenol Industrial Operations is a global leader in interconnect systems for harsh environment applications.

Micro-B connectors from Amphenol Industrial Operations are available from Newark.

Boilerplate

Boilerplate

Farnell Global is a fast and reliable distributor of products and technology for electronic and industrial system design, maintenance and repair. From research and design through prototype to production. Farnell Global helps its customers access the products and services they need 24/7. With more than 80 years of experience, 48 localised websites, and a dedicated team of over 3,000 employees, Farnell Global provides every component its customers need to build the technology of tomorrow.

Farnell Global trades as Newark in the Americas, Farnell in Europe, the Middle East, Africa and Japan, and element14 across Asia Pacific. It also sells through its CPC business in the UK.

Farnell Global has been part of the established global technology distributor, Avnet (Nasdaq: AVT), since 2016. Today, this relationship allows the company to support its customers at every stage of the product life cycle, offering a truly unique distribution model, as well as expertise in end-to-end delivery and product design.

For more information, visit http://www.farnell.com